Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSCastCondition.MiddlePlaneType |
TBSCastCondition.MiddlePlaneType.AUTOMATIC
Automatica determinaton of the central plane
|
static TBSCastCondition.MiddlePlaneType |
TBSCastCondition.MiddlePlaneType.AUTOMATIC_TIGHT
No holes are generated in the central plane
|
static TBSCastCondition.MiddlePlaneType |
TBSCastCondition.MiddlePlaneType.NONE
No definition of a central plane
|
static TBSCastCondition.MiddlePlaneType |
TBSCastCondition.MiddlePlaneType.POINT
A point within the central plane from which the deformation vector is positioned perpendicular to
|
static TBSCastCondition.MiddlePlaneType |
TBSCastCondition.MiddlePlaneType.STAMP
The element group is demolded keeping a stampable structure
|
static TBSCastCondition.MiddlePlaneType |
TBSCastCondition.MiddlePlaneType.SURFACE
The elements are demolded at the actual surface of the restrict area
|
Modifier and Type | Method and Description |
---|---|
TBSCastCondition.MiddlePlaneType |
TBSCastCondition.middlePlane()
Returns the middle plane
License requirements: None. |
static TBSCastCondition.MiddlePlaneType |
TBSCastCondition.MiddlePlaneType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSCastCondition.MiddlePlaneType |
TBSCastCondition.MiddlePlaneType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSCastCondition.MiddlePlaneType[] |
TBSCastCondition.MiddlePlaneType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSCastCondition.setMiddlePlane(TBSCastCondition.MiddlePlaneType middlePlane)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.