Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSBaseDesignVariableBuilder.GroupOperator |
TBSBaseDesignVariableBuilder.GroupOperator.COUNT
Determines the number of values of the selection area
|
static TBSBaseDesignVariableBuilder.GroupOperator |
TBSBaseDesignVariableBuilder.GroupOperator.DEVIATION
Deviation from the maximum value of the reference value
|
static TBSBaseDesignVariableBuilder.GroupOperator |
TBSBaseDesignVariableBuilder.GroupOperator.MAX
Maximum value fo the selection area
|
static TBSBaseDesignVariableBuilder.GroupOperator |
TBSBaseDesignVariableBuilder.GroupOperator.MIN
Minimum value of the selection area
|
static TBSBaseDesignVariableBuilder.GroupOperator |
TBSBaseDesignVariableBuilder.GroupOperator.SUM
Sum of all values of the selection area
|
Modifier and Type | Method and Description |
---|---|
TBSBaseDesignVariableBuilder.GroupOperator |
TBSBaseDesignVariableBuilder.groupOperatorOption()
Returns the group operator option
License requirements: None. |
static TBSBaseDesignVariableBuilder.GroupOperator |
TBSBaseDesignVariableBuilder.GroupOperator.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSBaseDesignVariableBuilder.GroupOperator |
TBSBaseDesignVariableBuilder.GroupOperator.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSBaseDesignVariableBuilder.GroupOperator[] |
TBSBaseDesignVariableBuilder.GroupOperator.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSBaseDesignVariableBuilder.setGroupOperatorOption(TBSBaseDesignVariableBuilder.GroupOperator groupOperatorOption)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.