Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static DAODesignVariableBuilder.Variable |
DAODesignVariableBuilder.Variable.ALL_EXPRESSIONS
Variables from FEM, SIM and master part
|
static DAODesignVariableBuilder.Variable |
DAODesignVariableBuilder.Variable.COUNT
Variable type count
|
static DAODesignVariableBuilder.Variable |
DAODesignVariableBuilder.Variable.FEATURE_DIMENSION
Feature dimension variables
|
static DAODesignVariableBuilder.Variable |
DAODesignVariableBuilder.Variable.SECTION_PROPERTY
Section property variables
|
static DAODesignVariableBuilder.Variable |
DAODesignVariableBuilder.Variable.SHELL_PROPERTY
Shell property variables
|
static DAODesignVariableBuilder.Variable |
DAODesignVariableBuilder.Variable.SKETCH_DIMENSION
Sketch dimension variables
|
DAODesignVariableBuilder.Variable |
DAODesignVariableBuilder.VariableData.variableType
Variable type
|
Modifier and Type | Method and Description |
---|---|
static DAODesignVariableBuilder.Variable |
DAODesignVariableBuilder.Variable.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DAODesignVariableBuilder.Variable |
DAODesignVariableBuilder.Variable.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DAODesignVariableBuilder.Variable[] |
DAODesignVariableBuilder.Variable.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DAODesignVariableBuilder.setVariable(DAODesignVariableBuilder.Variable variableType,
Expression variableExpression)
Sets the design variable
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.