Package | Description |
---|---|
nxopen.cae.modelcheck |
Provides classes and interfaces relating to Model Check.
|
Modifier and Type | Field and Description |
---|---|
static TestValueTypes.TestType |
TestValueTypes.TestType.AREA |
static TestValueTypes.TestType |
TestValueTypes.TestType.ASPECT_RATIO |
static TestValueTypes.TestType |
TestValueTypes.TestType.AXISYMMETRIC_X
When elements are modeled in XZ plane,
check X >= 0.0.
|
static TestValueTypes.TestType |
TestValueTypes.TestType.AXISYMMETRIC_Y
When elements are modeled in XZ plane,
check consistent Y.
|
static TestValueTypes.TestType |
TestValueTypes.TestType.COHESIVE_ELEMENT |
static TestValueTypes.TestType |
TestValueTypes.TestType.EDGE_POINT_INCLUDED_ANGLE |
static TestValueTypes.TestType |
TestValueTypes.TestType.EDGE_POINT_LENGTH_RATIO |
static TestValueTypes.TestType |
TestValueTypes.TestType.FACE_WARP_COEFFICIENT |
static TestValueTypes.TestType |
TestValueTypes.TestType.INTERIOR_ANGLE_MAXIMUM |
static TestValueTypes.TestType |
TestValueTypes.TestType.INTERIOR_ANGLE_MINIMUM |
static TestValueTypes.TestType |
TestValueTypes.TestType.JACOBIAN_RATIO |
static TestValueTypes.TestType |
TestValueTypes.TestType.JACOBIAN_SIGN |
static TestValueTypes.TestType |
TestValueTypes.TestType.JACOBIAN_ZERO |
static TestValueTypes.TestType |
TestValueTypes.TestType.LAMINATE_TAPER_RATIO
Ratio of longest edge to shortest edge in
stacking direction for the elements
that reference PCOMPS entries only.
|
static TestValueTypes.TestType |
TestValueTypes.TestType.LAMINATE_THICKNESS_RATIO
Ratio of the difference between thickness
in stacking direction as defined by grids
and thickness as defined by ply thickness
specification to the thickness in the stacking
direction as defined by grids for the elements
that reference PCOMPS entries only.
|
static TestValueTypes.TestType |
TestValueTypes.TestType.LENGTH_MAXIMUM |
static TestValueTypes.TestType |
TestValueTypes.TestType.LENGTH_MINIMUM |
static TestValueTypes.TestType |
TestValueTypes.TestType.LENGTH_RATIO_OFFSET |
static TestValueTypes.TestType |
TestValueTypes.TestType.PARALLEL_DEVIATION |
static TestValueTypes.TestType |
TestValueTypes.TestType.SHAPE_FACTOR |
static TestValueTypes.TestType |
TestValueTypes.TestType.SKEW_ANGLE |
static TestValueTypes.TestType |
TestValueTypes.TestType.TAPER |
TestValueTypes.TestType |
ElementQualityCheckResults.TestSummary.testType
the test type
|
static TestValueTypes.TestType |
TestValueTypes.TestType.TET_COLLAPSE |
static TestValueTypes.TestType |
TestValueTypes.TestType.TWIST |
static TestValueTypes.TestType |
TestValueTypes.TestType.VOLUME |
static TestValueTypes.TestType |
TestValueTypes.TestType.WARP_FACTOR |
static TestValueTypes.TestType |
TestValueTypes.TestType.WARPAGE_ANGLE |
Modifier and Type | Method and Description |
---|---|
TestValueTypes.TestType |
ITestValue.getTestType()
Returns the test type
License requirements: None. |
TestValueTypes.TestType |
TestResult.testType()
Returns the test type
License requirements: None. |
static TestValueTypes.TestType |
TestValueTypes.TestType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TestValueTypes.TestType |
TestValueTypes.TestType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TestValueTypes.TestType[] |
TestValueTypes.TestType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
QualityTestValue |
ElementQualitySetting.getTestValueByType(TestValueTypes.TestType testType)
|
String |
ElementQualitySetting.locateTestDescriptorName(FEElement element,
TestValueTypes.TestType testType,
boolean useElemSpecific)
Returns the name of a quality test value, which is associated with
an element for a specified test type
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Constructor and Description |
---|
TestSummary(TestValueTypes.TestType testTypeInitial,
double worstTestValueInitial,
boolean hasTestValueInitial,
int testCountInitial,
int errorCountInitial,
int warnedCountInitial)
Constructor for the TestSummary object.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.