Package | Description |
---|---|
nxopen.cae.modelcheck |
Provides classes and interfaces relating to Model Check.
|
Modifier and Type | Field and Description |
---|---|
static TestValueTypes.CriteriaType |
TestValueTypes.CriteriaType.ERROR
reports as error if the check result failed with the criteria value
|
static TestValueTypes.CriteriaType |
TestValueTypes.CriteriaType.WARNING
reports as warning if the check result failed with the criteria value
|
Modifier and Type | Method and Description |
---|---|
static TestValueTypes.CriteriaType |
TestValueTypes.CriteriaType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TestValueTypes.CriteriaType |
TestValueTypes.CriteriaType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TestValueTypes.CriteriaType[] |
TestValueTypes.CriteriaType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
ITestValue.CriteriaValueData |
ITestValue.getCriteriaValue(TestValueTypes.CriteriaType criteriaType)
Returns the criteria value.
|
void |
ITestValue.setCriteriaValue(TestValueTypes.CriteriaType criteriaType,
double criteriaValue,
Unit unit)
Sets the criteria value.
|
void |
ITestValue.setCriteriaValue(TestValueTypes.CriteriaType criteriaType,
String criteriaValue,
Unit unit)
Sets the criteria value.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.