Package | Description |
---|---|
nxopen.cae.modelcheck |
Provides classes and interfaces relating to Model Check.
|
Modifier and Type | Field and Description |
---|---|
static AlignShellElementFirstEdgeBuilder.ElemSelectionMode |
AlignShellElementFirstEdgeBuilder.ElemSelectionMode.ALL_VISIBLE_CONNECTED_SHELL_ELEMENTS |
static AlignShellElementFirstEdgeBuilder.ElemSelectionMode |
AlignShellElementFirstEdgeBuilder.ElemSelectionMode.CONNECTED_ELEMENTSIN_SEED_MESH |
static AlignShellElementFirstEdgeBuilder.ElemSelectionMode |
AlignShellElementFirstEdgeBuilder.ElemSelectionMode.SELECTED_CONNECTED_ELEMENTS |
Modifier and Type | Method and Description |
---|---|
AlignShellElementFirstEdgeBuilder.ElemSelectionMode |
AlignShellElementFirstEdgeBuilder.elemSelectionMethod()
Returns the element selection method
License requirements: None. |
static AlignShellElementFirstEdgeBuilder.ElemSelectionMode |
AlignShellElementFirstEdgeBuilder.ElemSelectionMode.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AlignShellElementFirstEdgeBuilder.ElemSelectionMode |
AlignShellElementFirstEdgeBuilder.ElemSelectionMode.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AlignShellElementFirstEdgeBuilder.ElemSelectionMode[] |
AlignShellElementFirstEdgeBuilder.ElemSelectionMode.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AlignShellElementFirstEdgeBuilder.setElemSelectionMethod(AlignShellElementFirstEdgeBuilder.ElemSelectionMode elemSelectionMethod)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.