public class CheckScope extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DISPLAYED
check all displayed elements or nodes
|
static int |
_SELECTED
check selected elements or nodes
|
static CheckScope |
DISPLAYED
check all displayed elements or nodes
|
static CheckScope |
SELECTED
check selected elements or nodes
|
Modifier and Type | Method and Description |
---|---|
static CheckScope |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CheckScope |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CheckScope[] |
values()
Returns an array that contains the values for this enum.
|
public static final CheckScope DISPLAYED
public static final CheckScope SELECTED
public static final int _DISPLAYED
public static final int _SELECTED
public static CheckScope valueOf(int value)
public static CheckScope valueOf(String name)
public static CheckScope[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.