Package | Description |
---|---|
nxopen.cae.ftk |
Provides classes and interfaces to Function Toolkit.
|
Modifier and Type | Field and Description |
---|---|
static DataManager.FileContainerType |
DataManager.FileContainerType.ALL
All containers
|
static DataManager.FileContainerType |
DataManager.FileContainerType.ASSOCIATED_CONTAINER
Part associated container which has the same simple name with the part
|
static DataManager.FileContainerType |
DataManager.FileContainerType.NONE
Not any container
|
static DataManager.FileContainerType |
DataManager.FileContainerType.RESULT_CONTAINER
Solution result container which has the same name with the solution
|
static DataManager.FileContainerType |
DataManager.FileContainerType.USER_CONTAINER
User container
|
Modifier and Type | Method and Description |
---|---|
static DataManager.FileContainerType |
DataManager.FileContainerType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DataManager.FileContainerType |
DataManager.FileContainerType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DataManager.FileContainerType[] |
DataManager.FileContainerType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DataManager.loadFile(String fileName,
DataManager.FileContainerType containerType)
Loads an AFU/OP2 file to the specified container.
|
void |
DataManager.unloadFile(String fileName,
DataManager.FileContainerType containerType)
Unloads an AFU/OP2 file from the specified container.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.