Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cae.ftk |
Provides classes and interfaces to Function Toolkit.
|
Modifier and Type | Field and Description |
---|---|
static XyFunctionMeasure |
XyFunctionMeasure.ACCELERATION
Acceleration unit
|
static XyFunctionMeasure |
XyFunctionMeasure.ANGULAR_ACCELERATION
Angular acceleration unit
|
static XyFunctionMeasure |
XyFunctionMeasure.ANGULAR_DISPLACEMENT
Angular displacement unit
|
static XyFunctionMeasure |
XyFunctionMeasure.ANGULAR_VELOCITY
Angular velocity unit
|
static XyFunctionMeasure |
XyFunctionMeasure.AREA
Area
|
static XyFunctionMeasure |
XyFunctionMeasure.CONVECTION_COEFFICIENT
Convection Coefficient
|
static XyFunctionMeasure |
XyFunctionMeasure.CURVATURE
Curvature unit
|
static XyFunctionMeasure |
XyFunctionMeasure.CYCLES
Cycles unit
|
static XyFunctionMeasure |
XyFunctionMeasure.DAMPING
Damping
|
static XyFunctionMeasure |
XyFunctionMeasure.DISPLACEMENT
Displacement unit
|
static XyFunctionMeasure |
XyFunctionMeasure.DYNAMIC_VISCOSITY
Dynamic Viscosity
|
static XyFunctionMeasure |
XyFunctionMeasure.ELECTRIC_CURRENT
Electric current unit
|
static XyFunctionMeasure |
XyFunctionMeasure.ELEMENT_FORCE
Element force unit
|
static XyFunctionMeasure |
XyFunctionMeasure.ELEMENT_MOMENT
Element moment unit
|
static XyFunctionMeasure |
XyFunctionMeasure.ENERGY
Energy
|
static XyFunctionMeasure |
XyFunctionMeasure.FORCE
Force unit
|
static XyFunctionMeasure |
XyFunctionMeasure.FREQUENCY
Frequency unit
|
static XyFunctionMeasure |
XyFunctionMeasure.GENERAL
General unit
|
static XyFunctionMeasure |
XyFunctionMeasure.GRAVITY
Gravity unit
|
static XyFunctionMeasure |
XyFunctionMeasure.HEAT_FLUX
Heat Flux
|
static XyFunctionMeasure |
XyFunctionMeasure.LENGTH_PER_ANGLE
Length Per Angle
|
static XyFunctionMeasure |
XyFunctionMeasure.LOADFACTOR
Load Factor unit
|
static XyFunctionMeasure |
XyFunctionMeasure.MASS
Mass unit
|
static XyFunctionMeasure |
XyFunctionMeasure.MASS_FLOW
Mass flow
|
static XyFunctionMeasure |
XyFunctionMeasure.MESS_DENSITY
mess density
|
static XyFunctionMeasure |
XyFunctionMeasure.MOMENT
Moment unit
|
static XyFunctionMeasure |
XyFunctionMeasure.MOMENT_PER_ANGLE
Moment Per Angle
|
static XyFunctionMeasure |
XyFunctionMeasure.MOTOR_SIGNAL
Motor signal unit
|
static XyFunctionMeasure |
XyFunctionMeasure.NUMBER
Measure number
|
static XyFunctionMeasure |
XyFunctionMeasure.ORDER
Order unit
|
static XyFunctionMeasure |
XyFunctionMeasure.POWER
Power
|
static XyFunctionMeasure |
XyFunctionMeasure.PRESSURE
Pressure unit
|
static XyFunctionMeasure |
XyFunctionMeasure.RPM
RPM unit
|
static XyFunctionMeasure |
XyFunctionMeasure.SPECIFIC_HEAT
specific heat
|
static XyFunctionMeasure |
XyFunctionMeasure.STRAIN
Strain unit
|
static XyFunctionMeasure |
XyFunctionMeasure.STRESS
Stress unit
|
static XyFunctionMeasure |
XyFunctionMeasure.TEMPERATURE
Temperature unit
|
static XyFunctionMeasure |
XyFunctionMeasure.THERMAL_CONDUCTIVITY
thermal conductivity
|
static XyFunctionMeasure |
XyFunctionMeasure.THERMAL_EXPANSION_COEFFICIENT
Thermal Expansion Coefficient
|
static XyFunctionMeasure |
XyFunctionMeasure.TIME
Time unit
|
static XyFunctionMeasure |
XyFunctionMeasure.TORQUE
Torque unit
|
static XyFunctionMeasure |
XyFunctionMeasure.UNITLESS_INTEGER
Unitless integer unit
|
static XyFunctionMeasure |
XyFunctionMeasure.UNITLESS_REAL
Unitless real unit
|
static XyFunctionMeasure |
XyFunctionMeasure.UNITLESS_SCALAR
Unitless scalar unit
|
static XyFunctionMeasure |
XyFunctionMeasure.VELOCITY
Velocity unit
|
static XyFunctionMeasure |
XyFunctionMeasure.VELOCITY_PER_PRESSURE
Velocity per Pressure
|
static XyFunctionMeasure |
XyFunctionMeasure.VOLTAGE
Voltage unit
|
Modifier and Type | Method and Description |
---|---|
static XyFunctionMeasure |
XyFunctionMeasure.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static XyFunctionMeasure |
XyFunctionMeasure.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static XyFunctionMeasure[] |
XyFunctionMeasure.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
BaseUnit |
DataManager.createArrayUnit(XyFunctionMeasure measureType,
XyFunctionUnit unitType)
Deprecated.
Deprecated in NX11.0.0. Use
DataManager.createArrayUnit(nxopen.Unit) instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.