Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static TransientResultsReductionBuilder.EvaluationError |
TransientResultsReductionBuilder.EvaluationError.ABORT |
static TransientResultsReductionBuilder.EvaluationError |
TransientResultsReductionBuilder.EvaluationError.SKIP |
static TransientResultsReductionBuilder.EvaluationError |
TransientResultsReductionBuilder.EvaluationError.ZERO_FILL |
Modifier and Type | Method and Description |
---|---|
static TransientResultsReductionBuilder.EvaluationError |
TransientResultsReductionBuilder.EvaluationError.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TransientResultsReductionBuilder.EvaluationError |
TransientResultsReductionBuilder.EvaluationError.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TransientResultsReductionBuilder.EvaluationError[] |
TransientResultsReductionBuilder.EvaluationError.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TransientResultsReductionBuilder.setEvaluationErrorOption(TransientResultsReductionBuilder.EvaluationError evaluationErrorOption)
Set evaluation error option
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.