Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SimSolution.StepPosition |
SimSolution.StepPosition.AFTER
after the specified step
|
static SimSolution.StepPosition |
SimSolution.StepPosition.BEFORE
before the specified step
|
static SimSolution.StepPosition |
SimSolution.StepPosition.FIRST
first
|
static SimSolution.StepPosition |
SimSolution.StepPosition.LAST
last
|
Modifier and Type | Method and Description |
---|---|
static SimSolution.StepPosition |
SimSolution.StepPosition.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimSolution.StepPosition |
SimSolution.StepPosition.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimSolution.StepPosition[] |
SimSolution.StepPosition.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
SimSolutionStep |
SimSolution.createStep(int stepType,
boolean makeActive,
String stepName,
SimSolution.StepPosition position,
SimSolutionStep relativeStep)
Create a step at the specified position, add to the solution and optionally make it active
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
SimSolution.moveStep(SimSolutionStep stepToMove,
SimSolution.StepPosition position,
SimSolutionStep relativeStep)
Moves step to the specified position
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.