Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SimSimulation.AxisymAbstractionType |
SimSimulation.AxisymAbstractionType.NONE
No axisymmetric elements are allowed
|
static SimSimulation.AxisymAbstractionType |
SimSimulation.AxisymAbstractionType.XXY_PLANE
XY plane - X axis axisymmetric elements are allowed
|
static SimSimulation.AxisymAbstractionType |
SimSimulation.AxisymAbstractionType.XY_PLANE
XY plane - Y axis axisymmetric elements are allowed
|
static SimSimulation.AxisymAbstractionType |
SimSimulation.AxisymAbstractionType.ZX_PLANE
ZX plane - Z axis axisymmetric elements are allowed
|
Modifier and Type | Method and Description |
---|---|
SimSimulation.AxisymAbstractionType |
SimSolution.abstractionType()
Returns the abstraction type
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
static SimSimulation.AxisymAbstractionType |
SimSimulation.AxisymAbstractionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimSimulation.AxisymAbstractionType |
SimSimulation.AxisymAbstractionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimSimulation.AxisymAbstractionType[] |
SimSimulation.AxisymAbstractionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
SimSolution |
SimSimulation.createSolution(String solverType,
String analysisType,
String solutionType,
String name,
SimSimulation.AxisymAbstractionType abstractionType)
Creates a solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.