Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SimLoadSet.Type |
SimLoadSet.Type.ACOUSTIC
Acoustic Load Set.
|
static SimLoadSet.Type |
SimLoadSet.Type.BOLT
Bolt Load Set.
|
static SimLoadSet.Type |
SimLoadSet.Type.FREQUENCY
Frequency Excitation Load Set.
|
static SimLoadSet.Type |
SimLoadSet.Type.INVALID
Static load set.
|
static SimLoadSet.Type |
SimLoadSet.Type.STATIC
Static load set.
|
static SimLoadSet.Type |
SimLoadSet.Type.TEMPERATURE
Temperature Set.
|
static SimLoadSet.Type |
SimLoadSet.Type.TRANSIENT
Transient Excitation Load Set.
|
Modifier and Type | Method and Description |
---|---|
SimLoadSet.Type |
SimLoadSet.loadSetType()
Returns the type of the load set
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
static SimLoadSet.Type |
SimLoadSet.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimLoadSet.Type |
SimLoadSet.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimLoadSet.Type[] |
SimLoadSet.Type.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.