Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SimLoadRecipeTypes.LoadConditionHandling |
SimLoadRecipeTypes.LoadConditionHandling.PER_DATA_SOURCE
Treat each source as a load condition
|
static SimLoadRecipeTypes.LoadConditionHandling |
SimLoadRecipeTypes.LoadConditionHandling.SINGLE
Treat all sources as a single load condition
|
Modifier and Type | Method and Description |
---|---|
SimLoadRecipeTypes.LoadConditionHandling |
SimLoadRecipe.getLoadConditionHandlingType()
Gets the type of load conditions handling of the
SimLoadRecipe
License requirements: None. |
static SimLoadRecipeTypes.LoadConditionHandling |
SimLoadRecipeTypes.LoadConditionHandling.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimLoadRecipeTypes.LoadConditionHandling |
SimLoadRecipeTypes.LoadConditionHandling.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimLoadRecipeTypes.LoadConditionHandling[] |
SimLoadRecipeTypes.LoadConditionHandling.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SimLoadRecipe.setLoadConditionHandlingType(SimLoadRecipeTypes.LoadConditionHandling lcHandling)
Sets the type of load conditions handling of the
SimLoadRecipe
License requirements: nx_masterfem ("Finite Element Modeling") Created in NX10.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.