Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SimLoadRecipeFunctionAttributes.CorrectionModes |
SimLoadRecipeFunctionAttributes.CorrectionModes.AMPLITUDE
Amplitude
|
static SimLoadRecipeFunctionAttributes.CorrectionModes |
SimLoadRecipeFunctionAttributes.CorrectionModes.ENERGY
Energy
|
static SimLoadRecipeFunctionAttributes.CorrectionModes |
SimLoadRecipeFunctionAttributes.CorrectionModes.UNKNOWN
Unkonwn
|
Modifier and Type | Method and Description |
---|---|
SimLoadRecipeFunctionAttributes.CorrectionModes |
SimLoadRecipeFunctionAttributes.correctionMode()
Returns the default correction mode of the functions in the file
License requirements: None. |
static SimLoadRecipeFunctionAttributes.CorrectionModes |
SimLoadRecipeFunctionAttributes.CorrectionModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimLoadRecipeFunctionAttributes.CorrectionModes |
SimLoadRecipeFunctionAttributes.CorrectionModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimLoadRecipeFunctionAttributes.CorrectionModes[] |
SimLoadRecipeFunctionAttributes.CorrectionModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SimLoadRecipeFunctionAttributes.setCorrectionMode(SimLoadRecipeFunctionAttributes.CorrectionModes correctionMode)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.