Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SimConditionSeqMgr.FileFormat |
SimConditionSeqMgr.FileFormat.BDD |
static SimConditionSeqMgr.FileFormat |
SimConditionSeqMgr.FileFormat.XML |
Modifier and Type | Method and Description |
---|---|
static SimConditionSeqMgr.FileFormat |
SimConditionSeqMgr.FileFormat.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimConditionSeqMgr.FileFormat |
SimConditionSeqMgr.FileFormat.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimConditionSeqMgr.FileFormat[] |
SimConditionSeqMgr.FileFormat.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SimConditionSeqMgr.exportFile(String filename,
SimConditionSeqMgr.FileFormat format)
Exports a
SimConditionSequence to a file on disk. |
void |
SimConditionSeqMgr.importFile(String filename,
SimConditionSeqMgr.FileFormat format)
Imports a file from disk to create a
SimConditionSequence . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.