Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SignalProcessingDBSettings.DBFormats |
SignalProcessingDBSettings.DBFormats.DB10
10
|
static SignalProcessingDBSettings.DBFormats |
SignalProcessingDBSettings.DBFormats.DB20
20
|
Modifier and Type | Method and Description |
---|---|
SignalProcessingDBSettings.DBFormats |
SignalProcessingDBSettings.dbformat()
Returns the dB format to apply
License requirements: None. |
static SignalProcessingDBSettings.DBFormats |
SignalProcessingDBSettings.DBFormats.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SignalProcessingDBSettings.DBFormats |
SignalProcessingDBSettings.DBFormats.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SignalProcessingDBSettings.DBFormats[] |
SignalProcessingDBSettings.DBFormats.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SignalProcessingDBSettings.setDBFormat(SignalProcessingDBSettings.DBFormats format)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.