Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ShellEADBuilder.MaterialOrientationMethod |
ShellEADBuilder.MaterialOrientationMethod.COORDINATE_SYSTEM
use a coordinate system to orient the material
|
static ShellEADBuilder.MaterialOrientationMethod |
ShellEADBuilder.MaterialOrientationMethod.COORDINATE_SYSTEM_DATA
use coordinate system raw data to orient the material
|
static ShellEADBuilder.MaterialOrientationMethod |
ShellEADBuilder.MaterialOrientationMethod.VECTOR_PROJECTION
use a vector projected to the shell to orient the material
|
Modifier and Type | Method and Description |
---|---|
ShellEADBuilder.MaterialOrientationMethod |
ShellEADBuilder.setMatOriMethod()
Returns the get selection ori operator gets material orientation method
License requirements: nx_masterfem ("Finite Element Modeling") . |
static ShellEADBuilder.MaterialOrientationMethod |
ShellEADBuilder.MaterialOrientationMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShellEADBuilder.MaterialOrientationMethod |
ShellEADBuilder.MaterialOrientationMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShellEADBuilder.MaterialOrientationMethod[] |
ShellEADBuilder.MaterialOrientationMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ShellEADBuilder.setSetMatOriMethod(ShellEADBuilder.MaterialOrientationMethod setMatOriMethod)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.