Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ResultProbeBuilder.CombineAcrossIterations |
ResultProbeBuilder.CombineAcrossIterations.ABSOLUTE_MAXIMUM |
static ResultProbeBuilder.CombineAcrossIterations |
ResultProbeBuilder.CombineAcrossIterations.ABSOLUTE_MINIMUM |
static ResultProbeBuilder.CombineAcrossIterations |
ResultProbeBuilder.CombineAcrossIterations.ARITHMETIC_MEAN |
static ResultProbeBuilder.CombineAcrossIterations |
ResultProbeBuilder.CombineAcrossIterations.MAXIMUM |
static ResultProbeBuilder.CombineAcrossIterations |
ResultProbeBuilder.CombineAcrossIterations.MINIMUM |
static ResultProbeBuilder.CombineAcrossIterations |
ResultProbeBuilder.CombineAcrossIterations.SUM |
Modifier and Type | Method and Description |
---|---|
ResultProbeBuilder.CombineAcrossIterations |
ResultProbeBuilder.combineIterOption()
Returns the combine option
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
static ResultProbeBuilder.CombineAcrossIterations |
ResultProbeBuilder.CombineAcrossIterations.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ResultProbeBuilder.CombineAcrossIterations |
ResultProbeBuilder.CombineAcrossIterations.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ResultProbeBuilder.CombineAcrossIterations[] |
ResultProbeBuilder.CombineAcrossIterations.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ResultProbeBuilder.setCombineIterOption(ResultProbeBuilder.CombineAcrossIterations combineOption)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.