Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
ResultParametersWithNodalForceReport |
ResultManager.createResultParametersWithNodalForceReport(NodalForceReport nodalForceReport)
Creates a result parameter object for given Free Body.
|
Modifier and Type | Method and Description |
---|---|
int |
Post.createPostview(int viewIndex,
ResultParametersWithNodalForceReport nodalforcereportparams)
Create a new post view for a given free body.
|
void |
ResultManager.deleteResultParametersWithNodalForceReport(ResultParametersWithNodalForceReport result)
Delete a
ResultParametersWithNodalForceReport object. |
void |
Post.postviewSetResultWithNodalForceReport(int postviewId,
ResultParametersWithNodalForceReport nodalforcereportparams)
Set the result for color display in the input for postview which is created with a free body
Post.createPostview(int, int, boolean) . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.