Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
ResultMeasureResultAllOptions
Represents the combination of all result options for result measure
To obtain an instance of this class use ResultMeasureCollection . |
interface |
ResultMeasureResultDirectionOptions
Represents the result directional options for result measure
To obtain an instance of this class use ResultMeasureCollection . |
interface |
ResultMeasureResultDirectionSectionOptions
Represents the result directional and beam/shell section options for result measure
To obtain an instance of this class use ResultMeasureCollection . |
interface |
ResultMeasureResultSectionOptions
Represents the result with beam/shell section options for result measure
To obtain an instance of this class use CAE#resultMeasureCollection . |
Modifier and Type | Method and Description |
---|---|
ResultMeasureResultOptions |
ResultMeasureCollection.createNewResultOptions(SimSolution tSol,
SimResultReference tResultReference,
Loadcase tResultLoadcase,
Iteration tResultIteration,
boolean bAllSubiterations,
Iteration tResultSubIteration,
Result.Type pType,
Result.Component eComp)
Create a result options for result measure
License requirements: nx_masterfem ("Finite Element Modeling") . |
ResultMeasureResultOptions |
ResultMeasureCollection.createResultOptions(SimSolution tSol,
int iStepIndex,
int iIterIndex,
Result.Type pType,
Result.Component eComp)
Deprecated.
|
ResultMeasureResultOptions |
ResultMeasureCollection.createResultOptionsNew(SimSolution tSol,
SimResultReference tResultReference,
int iStepIndex,
int iIterIndex,
Result.Type pType,
Result.Component eComp)
|
Modifier and Type | Method and Description |
---|---|
ResultMeasure |
ResultMeasureCollection.createResultMeasureNew(ResultMeasureResultOptions pResOpt,
ResultMeasureModelSubset pSubset,
String expName)
Create a ResultMeasure
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.