Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Result.SuperElementRep |
Result.SuperElementRep.SIMPLIFIED |
static Result.SuperElementRep |
Result.SuperElementRep.SYMBOLIC |
static Result.SuperElementRep |
Result.SuperElementRep.THREE_DIM |
Modifier and Type | Method and Description |
---|---|
Result.SuperElementRep[] |
Post.postviewAskSERepresentations(int postviewId,
int superelementId)
Gets all the representations of a super element in postivew.
|
static Result.SuperElementRep |
Result.SuperElementRep.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Result.SuperElementRep |
Result.SuperElementRep.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Result.SuperElementRep[] |
Result.SuperElementRep.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Post.postviewApplySERepresentation(int postviewId,
int[] superelementIds,
Result.SuperElementRep representation)
Set the representation of the multiple super elements in postivew.
|
void |
Post.postviewApplySERepresentation(int postviewId,
int superelementId,
Result.SuperElementRep representation)
Set the representation of the super element in postivew.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.