Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Result.Location |
Result.Location.ELEMENT |
static Result.Location |
Result.Location.ELEMENT_EDGE |
static Result.Location |
Result.Location.ELEMENT_EDGE_NODE |
static Result.Location |
Result.Location.ELEMENT_FACE |
static Result.Location |
Result.Location.ELEMENT_FACE_NODE |
static Result.Location |
Result.Location.ELEMENT_NODAL |
Result.Location |
ResultAccess.AskNMinMaxLocationData.location |
Result.Location |
ResultAccess.AskMinMaxLocationData.location |
Result.Location |
Result.Type.location |
static Result.Location |
Result.Location.NODAL |
Modifier and Type | Method and Description |
---|---|
Result.Location |
ResultAccess.askResultLocation()
Ask result location current result state.
|
Result.Location |
ResultParameters.getResultDataLocation()
Deprecated.
Deprecated in NX8.0.0. Use
BaseResultType.location() instead.
|
Result.Location |
ResultVariable.loc()
Returns the Location
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Result.Location |
BaseResultType.location()
Returns the
Result.Location where this result type is defined
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") OR sc_results_viewer (" Simcenter Results Viewer") Created in NX7.5.0 |
static Result.Location |
Result.Location.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Result.Location |
Result.Location.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Result.Location[] |
Result.Location.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
ResultVariable |
ResultManager.createResultvariable(SimSimulation sim,
Result.Quantity quan,
Result.Location loc,
Result.Component comp,
String restypename,
String name)
Creates Result Variable object
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") OR sc_results_viewer (" Simcenter Results Viewer") . |
void |
ResultVariable.setLoc(Result.Location loc)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultParameters.setResultDataLocation(Result.Location location)
Deprecated.
Deprecated in NX8.0.0. Use
ResultParameters.getGenericResultType() instead.
|
Constructor and Description |
---|
Type(Result.Quantity quantityInitial,
Result.Location locationInitial,
Result.Section sectionInitial)
Constructor for the Type object.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.