Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static RadiusType |
RadiusType.ALL_TYPES
All fillet types
|
static RadiusType |
RadiusType.INSIDE
inside radius
|
static RadiusType |
RadiusType.OUTSIDE
outside radius
|
Modifier and Type | Method and Description |
---|---|
static RadiusType |
RadiusType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RadiusType |
RadiusType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RadiusType[] |
RadiusType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
FilletFaceMethod |
SmartSelectionManager.createFilletFaceMethod(CAEBody[] seeds,
boolean doEntityVisibilityCheck,
RadiusType radiusType,
double dMinFilletRadius,
double dMaxFilletRadius,
double dMinFilletAngle,
double dMaxFilletAngle)
Creates a fillet face method
License requirements: nx_masterfem ("Finite Element Modeling") . |
FilletFaceMethod |
SmartSelectionManager.createFilletFaceMethod(CAEBody[] seeds,
RadiusType radiusType,
double dMinFilletRadius,
double dMaxFilletRadius,
double dMinFilletAngle,
double dMaxFilletAngle)
Deprecated.
Deprecated in NX11.0.0. Use overloaded
SmartSelectionManager.createFilletFaceMethod(nxopen.cae.CAEBody, nxopen.cae.RadiusType, double, double, double, double) which takes as input an array of CAEBody objects and the argument doEntityVisibilityCheck.
|
FilletFaceMethod |
SmartSelectionManager.createFilletFaceMethod(CAEBody seed,
RadiusType radiusType,
double dMinFilletRadius,
double dMaxFilletRadius,
double dMinFilletAngle,
double dMaxFilletAngle)
Deprecated.
Deprecated in NX11.0.0. Use overloaded
SmartSelectionManager.createFilletFaceMethod(nxopen.cae.CAEBody, nxopen.cae.RadiusType, double, double, double, double) which takes as input an array of CAEBody objects and the argument doEntityVisibilityCheck.
|
FilletFaceMethod |
SmartSelectionManager.createFilletFaceMethod(CAEFace[] seeds,
boolean doEntityVisibilityCheck,
RadiusType radiusType,
double dMinFilletRadius,
double dMaxFilletRadius,
double dMinFilletAngle,
double dMaxFilletAngle)
Creates a fillet face method
License requirements: nx_masterfem ("Finite Element Modeling") . |
FilletFaceMethod |
SmartSelectionManager.createFilletFaceMethod(CAEFace[] seeds,
RadiusType radiusType,
double dMinFilletRadius,
double dMaxFilletRadius,
double dMinFilletAngle,
double dMaxFilletAngle)
Deprecated.
Deprecated in NX11.0.0. Use overloaded
SmartSelectionManager.createFilletFaceMethod(nxopen.cae.CAEBody, nxopen.cae.RadiusType, double, double, double, double) which takes as input an array of CAEFace objects and the argument doEntityVisibilityCheck.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.