Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ProjectNodesToCadGeometryBuilder.ListingOption |
ProjectNodesToCadGeometryBuilder.ListingOption.ALL
List All information on nodes that are off the CAD geometry by more than the input tolerance
|
static ProjectNodesToCadGeometryBuilder.ListingOption |
ProjectNodesToCadGeometryBuilder.ListingOption.NONE
List nothing
|
static ProjectNodesToCadGeometryBuilder.ListingOption |
ProjectNodesToCadGeometryBuilder.ListingOption.SUMMARY_ONLY
List only Summary information
|
Modifier and Type | Method and Description |
---|---|
ProjectNodesToCadGeometryBuilder.ListingOption |
ProjectNodesToCadGeometryBuilder.listingOptionState()
Returns the listing option
License requirements: nx_masterfem ("Finite Element Modeling") . |
static ProjectNodesToCadGeometryBuilder.ListingOption |
ProjectNodesToCadGeometryBuilder.ListingOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ProjectNodesToCadGeometryBuilder.ListingOption |
ProjectNodesToCadGeometryBuilder.ListingOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ProjectNodesToCadGeometryBuilder.ListingOption[] |
ProjectNodesToCadGeometryBuilder.ListingOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ProjectNodesToCadGeometryBuilder.setListingOptionState(ProjectNodesToCadGeometryBuilder.ListingOption option)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.