Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PreTestSensorConfigBuilder.AlgorithmChoiceType |
PreTestSensorConfigBuilder.AlgorithmChoiceType.MIN_MAC |
Modifier and Type | Method and Description |
---|---|
PreTestSensorConfigBuilder.AlgorithmChoiceType |
PreTestSensorConfigBuilder.algorithmChoice()
Returns the sensor selection algorithm
License requirements: None. |
static PreTestSensorConfigBuilder.AlgorithmChoiceType |
PreTestSensorConfigBuilder.AlgorithmChoiceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PreTestSensorConfigBuilder.AlgorithmChoiceType |
PreTestSensorConfigBuilder.AlgorithmChoiceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PreTestSensorConfigBuilder.AlgorithmChoiceType[] |
PreTestSensorConfigBuilder.AlgorithmChoiceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PreTestSensorConfigBuilder.setAlgorithmChoice(PreTestSensorConfigBuilder.AlgorithmChoiceType algorithmChoice)
License requirements: nx_correl_base ("FE Correlation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.