Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PreTestExportUnvBuilder.FileUnitsOption |
PreTestExportUnvBuilder.FileUnitsOption.BA
BA: Foot (poundal)
|
static PreTestExportUnvBuilder.FileUnitsOption |
PreTestExportUnvBuilder.FileUnitsOption.BG
BG: Foot (pound f)
|
static PreTestExportUnvBuilder.FileUnitsOption |
PreTestExportUnvBuilder.FileUnitsOption.CM
CM: cm (centi newton)
|
static PreTestExportUnvBuilder.FileUnitsOption |
PreTestExportUnvBuilder.FileUnitsOption.GM
GM: mm (kilogram f)
|
static PreTestExportUnvBuilder.FileUnitsOption |
PreTestExportUnvBuilder.FileUnitsOption.IN
IN: Inch (pound f)
|
static PreTestExportUnvBuilder.FileUnitsOption |
PreTestExportUnvBuilder.FileUnitsOption.MG
MG: Meter (kilogram f)
|
static PreTestExportUnvBuilder.FileUnitsOption |
PreTestExportUnvBuilder.FileUnitsOption.MM
MM: mm (milli newton)
|
static PreTestExportUnvBuilder.FileUnitsOption |
PreTestExportUnvBuilder.FileUnitsOption.MN
MN: mm (newton)
|
static PreTestExportUnvBuilder.FileUnitsOption |
PreTestExportUnvBuilder.FileUnitsOption.SI
SI: Meter (newton)
|
Modifier and Type | Method and Description |
---|---|
PreTestExportUnvBuilder.FileUnitsOption |
PreTestExportUnvBuilder.nativeFileUnits()
Returns the native file units
License requirements: None. |
static PreTestExportUnvBuilder.FileUnitsOption |
PreTestExportUnvBuilder.FileUnitsOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PreTestExportUnvBuilder.FileUnitsOption |
PreTestExportUnvBuilder.FileUnitsOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PreTestExportUnvBuilder.FileUnitsOption[] |
PreTestExportUnvBuilder.FileUnitsOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PreTestExportUnvBuilder.setNativeFileUnits(PreTestExportUnvBuilder.FileUnitsOption nativeFileUnits)
License requirements: nx_correl_base ("FE Correlation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.