Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PreTestExciterConfigBuilder.MethodChoiceType |
PreTestExciterConfigBuilder.MethodChoiceType.AUTOMATIC_NMIF |
static PreTestExciterConfigBuilder.MethodChoiceType |
PreTestExciterConfigBuilder.MethodChoiceType.MANUAL |
Modifier and Type | Method and Description |
---|---|
PreTestExciterConfigBuilder.MethodChoiceType |
PreTestExciterConfigBuilder.methodChoice()
Returns the exciter selection method
License requirements: None. |
static PreTestExciterConfigBuilder.MethodChoiceType |
PreTestExciterConfigBuilder.MethodChoiceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PreTestExciterConfigBuilder.MethodChoiceType |
PreTestExciterConfigBuilder.MethodChoiceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PreTestExciterConfigBuilder.MethodChoiceType[] |
PreTestExciterConfigBuilder.MethodChoiceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PreTestExciterConfigBuilder.setMethodChoice(PreTestExciterConfigBuilder.MethodChoiceType algorithmChoice)
License requirements: nx_correl_base ("FE Correlation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.