Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PostGraphBuilder.EvalutionErrors |
PostGraphBuilder.EvalutionErrors.ABORT |
static PostGraphBuilder.EvalutionErrors |
PostGraphBuilder.EvalutionErrors.SKIP |
static PostGraphBuilder.EvalutionErrors |
PostGraphBuilder.EvalutionErrors.USER_VALUE |
Modifier and Type | Method and Description |
---|---|
PostGraphBuilder.EvalutionErrors |
PostGraphBuilder.evalutionErrorsOption()
Returns the error handling option when there are evaluation errors on selected entities or path
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") OR sc_results_viewer (" Simcenter Results Viewer") . |
static PostGraphBuilder.EvalutionErrors |
PostGraphBuilder.EvalutionErrors.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PostGraphBuilder.EvalutionErrors |
PostGraphBuilder.EvalutionErrors.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PostGraphBuilder.EvalutionErrors[] |
PostGraphBuilder.EvalutionErrors.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PostGraphBuilder.setEvalutionErrorsOption(PostGraphBuilder.EvalutionErrors evalutionErrorsOption)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") OR sc_results_viewer (" Simcenter Results Viewer") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.