Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PostGraphBuilder.EntityType |
PostGraphBuilder.EntityType.BODY |
static PostGraphBuilder.EntityType |
PostGraphBuilder.EntityType.EDGE |
static PostGraphBuilder.EntityType |
PostGraphBuilder.EntityType.ELEMENT |
static PostGraphBuilder.EntityType |
PostGraphBuilder.EntityType.FACE |
static PostGraphBuilder.EntityType |
PostGraphBuilder.EntityType.NODE |
static PostGraphBuilder.EntityType |
PostGraphBuilder.EntityType.POINT |
Modifier and Type | Method and Description |
---|---|
PostGraphBuilder.EntityType |
PostGraphBuilder.selectedEntityType()
Returns the entity type of the tags of entities which passed using SetEntityObjects function
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") OR sc_results_viewer (" Simcenter Results Viewer") . |
static PostGraphBuilder.EntityType |
PostGraphBuilder.EntityType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PostGraphBuilder.EntityType |
PostGraphBuilder.EntityType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PostGraphBuilder.EntityType[] |
PostGraphBuilder.EntityType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PostGraphBuilder.setSelectedEntityType(PostGraphBuilder.EntityType geometryEntity)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") OR sc_results_viewer (" Simcenter Results Viewer") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.