Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Post.Style |
Post.Style.ARROWS |
static Post.Style |
Post.Style.BANDED_CONTOURS |
static Post.Style |
Post.Style.CUBES |
static Post.Style |
Post.Style.ELEMENTS |
static Post.Style |
Post.Style.ISO_LINES |
static Post.Style |
Post.Style.ISO_SURFACES |
static Post.Style |
Post.Style.SMOOTH_CONTOURS |
static Post.Style |
Post.Style.SPHERES |
static Post.Style |
Post.Style.STREAMLINES |
static Post.Style |
Post.Style.TENSORS |
Modifier and Type | Method and Description |
---|---|
static Post.Style |
Post.Style.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.Style |
Post.Style.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.Style[] |
Post.Style.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Post.postviewSetStyle(int postviewId,
int showStyle,
Post.Style style)
Set the fringe style in the input postview id.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.