Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Post.StreamlineDirection |
Post.StreamlineDirection.BOTH |
Post.StreamlineDirection |
Post.StreamlineExtraction.direction |
static Post.StreamlineDirection |
Post.StreamlineDirection.DOWNSTREAM |
static Post.StreamlineDirection |
Post.StreamlineDirection.UPSTREAM |
Modifier and Type | Method and Description |
---|---|
static Post.StreamlineDirection |
Post.StreamlineDirection.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.StreamlineDirection |
Post.StreamlineDirection.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.StreamlineDirection[] |
Post.StreamlineDirection.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
StreamlineExtraction(Post.StreamlineDirection directionInitial,
double maximumTimeElapsedInitial,
int maxIntegrationStepsInitial,
boolean limitStepSizeInitial,
double maximumStepSizeInitial,
Post.IntegrationScheme integrationSchemeInitial,
boolean disjointRestartInitial)
Constructor for the StreamlineExtraction object.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.