Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Post.ShowHeader |
Post.ShowHeader.AUTOMATIC |
static Post.ShowHeader |
Post.ShowHeader.COMPACT |
static Post.ShowHeader |
Post.ShowHeader.CUSTOMIZED |
static Post.ShowHeader |
Post.ShowHeader.NONE |
Modifier and Type | Method and Description |
---|---|
Post.ShowHeader |
Post.postviewGetShowHeader(int postviewId)
Get show header option in the input postview id.
|
static Post.ShowHeader |
Post.ShowHeader.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.ShowHeader |
Post.ShowHeader.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.ShowHeader[] |
Post.ShowHeader.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Post.postviewSetShowHeader(int postviewId,
Post.ShowHeader showHeader)
Set show header option in the input postview id.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.