Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
Post.MarkSize |
Post.Mark.markSize |
static Post.MarkSize |
Post.MarkSize.RESULT_VALUE |
static Post.MarkSize |
Post.MarkSize.SPECIFIED |
Modifier and Type | Method and Description |
---|---|
static Post.MarkSize |
Post.MarkSize.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.MarkSize |
Post.MarkSize.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.MarkSize[] |
Post.MarkSize.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
Mark(boolean showArrowXComponentInitial,
boolean showArrowYComponentInitial,
boolean showArrowZComponentInitial,
boolean showArrowMagnitudeInitial,
Post.MarkRenderStyle markRenderStyleInitial,
Post.MarkTensorStyle markTensorStyleInitial,
Post.MarkColor markColorInitial,
NXColor specifiedColorInitial,
Post.MarkSize markSizeInitial,
Post.MarkMaximumSize markMaximumSizeInitial,
double modelPrecentValueInitial,
double specifiedLengthValueInitial,
Post.MarkLocation markLocationInitial,
boolean hideMarksBelowInitial,
Post.MarkHide belowMarkHideTypeInitial,
double belowResultPercentInitial,
double belowResultValueInitial,
boolean displayNumericalValueWithArrowInitial)
Constructor for the Mark object.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.