Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
Post.GraphIds |
Post.createHistoryGraph(int postviewId,
String name,
Post.GraphParameters graph,
int startIteration,
int endIteration,
int iterationIncrement,
int nodeLabel,
double[] point)
Create a graph by extracting data from the input postview id, at the input node label or point,
for the input iterations.
|
Post.GraphIds |
Post.createSpatialGraph(int postviewId,
String name,
Post.GraphParameters graph,
int pathId)
Create a graph by extracting data from the input postview id, along an input path id
The input postview id is what was returned from CreatePostview or CreatePostviewForResult.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.