Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Post.Export |
Post.Export.ASCII |
static Post.Export |
Post.Export.JT |
static Post.Export |
Post.Export.VRML |
Modifier and Type | Method and Description |
---|---|
static Post.Export |
Post.Export.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.Export |
Post.Export.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.Export[] |
Post.Export.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Post.postviewExportDisplay(int postviewId,
String fileName,
Post.Export format,
boolean ignoreClipping,
boolean ignoreVisibility)
Export the display of the input postview id to the specified format.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.