Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
Post.Colorbar |
Post.PostviewGetColorbarData.colorbar |
Modifier and Type | Method and Description |
---|---|
void |
Post.postviewSetColorbar(int postviewId,
Post.Colorbar colorbar)
Set colorbar options in the input postview id.
|
void |
Post.postviewSetColorbar(int postviewId,
Post.Colorbar colorbar,
boolean customOverwrite,
double[] rangeValue,
NXColor.Rgb[] rangeColors)
Set color bar options along with custom overwrite options in the input postview id.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.