Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Post.BandStyle |
Post.BandStyle.DEFAULT |
static Post.BandStyle |
Post.BandStyle.LINE |
static Post.BandStyle |
Post.BandStyle.VAL_INLINE |
Modifier and Type | Method and Description |
---|---|
static Post.BandStyle |
Post.BandStyle.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.BandStyle |
Post.BandStyle.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.BandStyle[] |
Post.BandStyle.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Post.postviewSetBandStyle(int postviewId,
Post.BandStyle bandstyle)
Set the band style in the input postview id.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.