Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PolygonGeometryManager.PolygonBodyResolutionType |
PolygonGeometryManager.PolygonBodyResolutionType.HIGH |
static PolygonGeometryManager.PolygonBodyResolutionType |
PolygonGeometryManager.PolygonBodyResolutionType.MEDIUM |
static PolygonGeometryManager.PolygonBodyResolutionType |
PolygonGeometryManager.PolygonBodyResolutionType.STANDARD |
Modifier and Type | Method and Description |
---|---|
PolygonGeometryManager.PolygonBodyResolutionType |
PolygonGeometryManager.getPolygonBodyResolutionOnFemBodies()
Gets the tesselation on polygon bodies that were created from CAD bodies.
|
static PolygonGeometryManager.PolygonBodyResolutionType |
PolygonGeometryManager.PolygonBodyResolutionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PolygonGeometryManager.PolygonBodyResolutionType |
PolygonGeometryManager.PolygonBodyResolutionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PolygonGeometryManager.PolygonBodyResolutionType[] |
PolygonGeometryManager.PolygonBodyResolutionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PolygonGeometryManager.setPolygonBodyResolutionOnFemBodies(PolygonGeometryManager.PolygonBodyResolutionType resType)
Sets the tesselation on polygon bodies that were created from CAD bodies.
|
CAEBody[] |
PolygonGeometryManager.setPolygonBodyResolutionWithRecreate(PolygonGeometryManager.PolygonBodyResolutionType resolutionType,
CAEBody[] inPolygonBodies)
Set Resolution for polygon body with recreate body only
License requirements: nx_masterfem ("Finite Element Modeling") . |
CAEBody[] |
PolygonGeometryManager.setPolygonBodyResolutionWithRecreateAndUpdate(PolygonGeometryManager.PolygonBodyResolutionType resolutionType,
CAEBody[] inPolygonBodies)
Set Resolution for polygon body with recreate body and update only
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.