Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PolygonFaceOnMeshBuilder.SelectBodyMethod |
PolygonFaceOnMeshBuilder.SelectBodyMethod.ADD_TO_EXISTING
Add to existing body
|
static PolygonFaceOnMeshBuilder.SelectBodyMethod |
PolygonFaceOnMeshBuilder.SelectBodyMethod.CREATE_NEW
Create new body
|
Modifier and Type | Method and Description |
---|---|
PolygonFaceOnMeshBuilder.SelectBodyMethod |
PolygonFaceOnMeshBuilder.selectBodyOption()
Returns the select body option for different ways of body select method
License requirements: None. |
static PolygonFaceOnMeshBuilder.SelectBodyMethod |
PolygonFaceOnMeshBuilder.SelectBodyMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PolygonFaceOnMeshBuilder.SelectBodyMethod |
PolygonFaceOnMeshBuilder.SelectBodyMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PolygonFaceOnMeshBuilder.SelectBodyMethod[] |
PolygonFaceOnMeshBuilder.SelectBodyMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PolygonFaceOnMeshBuilder.setSelectBodyOption(PolygonFaceOnMeshBuilder.SelectBodyMethod selectBodyMethod)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.