Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static NodalForceReport.SubcaseOption |
NodalForceReport.SubcaseOption.USE_ALL |
static NodalForceReport.SubcaseOption |
NodalForceReport.SubcaseOption.USE_SINGLE |
Modifier and Type | Method and Description |
---|---|
static NodalForceReport.SubcaseOption |
NodalForceReport.SubcaseOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NodalForceReport.SubcaseOption |
NodalForceReport.SubcaseOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NodalForceReport.SubcaseOption[] |
NodalForceReport.SubcaseOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
SimSolution |
SimSimulation.createSolution(NodalForceReport nodalForceReport,
String name,
NodalForceReport.SubcaseOption subcaseOption,
SimSolutionStep stepTag,
boolean createForce,
boolean createMoment)
Creates a solution from free body
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.