Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static MorphRevolvedMeshBuilder.CurveType |
MorphRevolvedMeshBuilder.CurveType.EDGE_CURVE
edge or curve
|
static MorphRevolvedMeshBuilder.CurveType |
MorphRevolvedMeshBuilder.CurveType.LINE
line segment
|
Modifier and Type | Method and Description |
---|---|
MorphRevolvedMeshBuilder.CurveType |
MorphRevolvedMeshBuilder.targetCurveType()
Returns the curve type
License requirements: None. |
static MorphRevolvedMeshBuilder.CurveType |
MorphRevolvedMeshBuilder.CurveType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MorphRevolvedMeshBuilder.CurveType |
MorphRevolvedMeshBuilder.CurveType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MorphRevolvedMeshBuilder.CurveType[] |
MorphRevolvedMeshBuilder.CurveType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MorphRevolvedMeshBuilder.setTargetCurveType(MorphRevolvedMeshBuilder.CurveType targetCurveType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.