Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ModelDisplayBuilder.NodeDisplayModeType |
ModelDisplayBuilder.NodeDisplayModeType.EXPLICIT
Nodes are explicitly shown and hidden via the Show/Hide commands.
|
static ModelDisplayBuilder.NodeDisplayModeType |
ModelDisplayBuilder.NodeDisplayModeType.IMPLICIT
Nodes are implicitly shown according to the following rules.
|
Modifier and Type | Method and Description |
---|---|
ModelDisplayBuilder.NodeDisplayModeType |
ModelDisplayBuilder.nodeDisplayMode()
Returns the node display mode type
License requirements: nx_masterfem ("Finite Element Modeling") . |
static ModelDisplayBuilder.NodeDisplayModeType |
ModelDisplayBuilder.NodeDisplayModeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ModelDisplayBuilder.NodeDisplayModeType |
ModelDisplayBuilder.NodeDisplayModeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ModelDisplayBuilder.NodeDisplayModeType[] |
ModelDisplayBuilder.NodeDisplayModeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ModelDisplayBuilder.setNodeDisplayMode(ModelDisplayBuilder.NodeDisplayModeType nodeDisplayMode)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.