Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static MeshPointProjectBuilder.ProjectionMethod |
MeshPointProjectBuilder.ProjectionMethod.TYPE_ALONG_VECTOR |
static MeshPointProjectBuilder.ProjectionMethod |
MeshPointProjectBuilder.ProjectionMethod.TYPE_NEAREST_POINT |
Modifier and Type | Method and Description |
---|---|
MeshPointProjectBuilder.ProjectionMethod |
MeshPointProjectBuilder.projectionOption()
Returns the projection method type
License requirements: None. |
static MeshPointProjectBuilder.ProjectionMethod |
MeshPointProjectBuilder.ProjectionMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeshPointProjectBuilder.ProjectionMethod |
MeshPointProjectBuilder.ProjectionMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeshPointProjectBuilder.ProjectionMethod[] |
MeshPointProjectBuilder.ProjectionMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MeshPointProjectBuilder.setProjectionOption(MeshPointProjectBuilder.ProjectionMethod projectionType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.