Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
MeshPoint |
MeshPointCollection.findObject(String journalIdentifier)
Finds the
MeshPoint with the given identifier as recorded in a journal. |
MeshPoint |
MeshPointBaseBuilder.meshPointToEdit()
Returns the base mesh point that will be replaced or edited after the commit operation (Edit Operation).
|
Modifier and Type | Method and Description |
---|---|
void |
OrderedSelection.add(MeshPoint entity)
Adds a mesh point to the list
License requirements: None. |
RelatedNodeMethod |
SmartSelectionManager.createRelatedNodeMethod(MeshPoint[] seedTags)
Deprecated.
Deprecated in NX11.0.0. Use overloaded
SmartSelectionManager.createRelatedNodeMethod(nxopen.cae.Mesh) which takes as input an array of MeshPoint objects and the argument doEntityVisibilityCheck.
|
RelatedNodeMethod |
SmartSelectionManager.createRelatedNodeMethod(MeshPoint[] seedTags,
boolean doEntityVisibilityCheck)
Creates a related node method
License requirements: nx_masterfem ("Finite Element Modeling") . |
RelatedNodeMethod |
SmartSelectionManager.createRelatedNodeMethod(MeshPoint seed,
boolean doEntityVisibilityCheck)
Creates a related node method
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
MeshPointBaseBuilder.setMeshPointToEdit(MeshPoint inMeshPoint)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.