Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static MechanicalLoadSumBuilder.UserUnit |
MechanicalLoadSumBuilder.UserUnit.DECK_UNIT
Load unit = same as Solver Deck Unit
|
static MechanicalLoadSumBuilder.UserUnit |
MechanicalLoadSumBuilder.UserUnit.FT_POUND_FORCE
Load unit = "lbf", Moment unit lbf-ft
|
static MechanicalLoadSumBuilder.UserUnit |
MechanicalLoadSumBuilder.UserUnit.IN_POUND_FORCE
Load unit = "lbf", Moment unit lbf-in
|
static MechanicalLoadSumBuilder.UserUnit |
MechanicalLoadSumBuilder.UserUnit.METER_NEWTON
Load unit = "N", Moment unit N-m
|
static MechanicalLoadSumBuilder.UserUnit |
MechanicalLoadSumBuilder.UserUnit.MILLI_MILLINEWTON
Load unit = "mN", Moment unit N-mm
|
static MechanicalLoadSumBuilder.UserUnit |
MechanicalLoadSumBuilder.UserUnit.MILLI_NEWTON
Load unit = "N", Moment unit N-mm
|
Modifier and Type | Method and Description |
---|---|
MechanicalLoadSumBuilder.UserUnit |
MechanicalLoadSumBuilder.userSpecifiedUnit()
Returns the output result unit
License requirements: None. |
static MechanicalLoadSumBuilder.UserUnit |
MechanicalLoadSumBuilder.UserUnit.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MechanicalLoadSumBuilder.UserUnit |
MechanicalLoadSumBuilder.UserUnit.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MechanicalLoadSumBuilder.UserUnit[] |
MechanicalLoadSumBuilder.UserUnit.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MechanicalLoadSumBuilder.setUserSpecifiedUnit(MechanicalLoadSumBuilder.UserUnit userSpecifiedUnit)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.