Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ManualMorphBuilder.MapMethod |
ManualMorphBuilder.MapMethod.ALONG_ELEMENT_NORMAL |
static ManualMorphBuilder.MapMethod |
ManualMorphBuilder.MapMethod.ALONG_VECTOR |
static ManualMorphBuilder.MapMethod |
ManualMorphBuilder.MapMethod.BASED_ON_EDGE_NODE_MOVEMENT |
static ManualMorphBuilder.MapMethod |
ManualMorphBuilder.MapMethod.KEEP_SOURCE_BIAS |
static ManualMorphBuilder.MapMethod |
ManualMorphBuilder.MapMethod.NEAREST_POINT |
static ManualMorphBuilder.MapMethod |
ManualMorphBuilder.MapMethod.UNIFORM_ACROSS_EDGE |
Modifier and Type | Method and Description |
---|---|
static ManualMorphBuilder.MapMethod |
ManualMorphBuilder.MapMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ManualMorphBuilder.MapMethod |
ManualMorphBuilder.MapMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ManualMorphBuilder.MapMethod[] |
ManualMorphBuilder.MapMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ManualMorphBuilder.setMapMethod(TaggedObject mapDataTag,
ManualMorphBuilder.MapMethod mapMethod)
Sets the method chosen to apply node mapping on selected geometry
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.