Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static LbcAssociationMgr.BcType |
LbcAssociationMgr.BcType.CONSTRAINT
Associate constraints
|
static LbcAssociationMgr.BcType |
LbcAssociationMgr.BcType.LOAD
Associate loads
|
static LbcAssociationMgr.BcType |
LbcAssociationMgr.BcType.NONE
no valid type
|
static LbcAssociationMgr.BcType |
LbcAssociationMgr.BcType.SIMULATION_OBJECT
Associate simulation objects
|
Modifier and Type | Method and Description |
---|---|
LbcAssociationMgr.BcType |
LbcAssociationMgr.typeOption()
Returns the bc type option
License requirements: None. |
static LbcAssociationMgr.BcType |
LbcAssociationMgr.BcType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LbcAssociationMgr.BcType |
LbcAssociationMgr.BcType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LbcAssociationMgr.BcType[] |
LbcAssociationMgr.BcType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LbcAssociationMgr.setTypeOption(LbcAssociationMgr.BcType entityOption)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.