Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static LaminateSpreadsheetReportBuilder.SolverInputType |
LaminateSpreadsheetReportBuilder.SolverInputType.PLY_STRESS
Use the solver ply stresses
|
static LaminateSpreadsheetReportBuilder.SolverInputType |
LaminateSpreadsheetReportBuilder.SolverInputType.SHELL_STRESS
Use the solver shell stress resultants
|
Modifier and Type | Method and Description |
---|---|
LaminateSpreadsheetReportBuilder.SolverInputType |
LaminateSpreadsheetReportBuilder.solverInput()
Returns the solver input
License requirements: None. |
static LaminateSpreadsheetReportBuilder.SolverInputType |
LaminateSpreadsheetReportBuilder.SolverInputType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LaminateSpreadsheetReportBuilder.SolverInputType |
LaminateSpreadsheetReportBuilder.SolverInputType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LaminateSpreadsheetReportBuilder.SolverInputType[] |
LaminateSpreadsheetReportBuilder.SolverInputType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LaminateSpreadsheetReportBuilder.setSolverInput(LaminateSpreadsheetReportBuilder.SolverInputType solverInput)
License requirements: nx_lam_composites ("Laminate Composites") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.