Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static LaminateSpreadsheetReportBuilder.FailureModeType |
LaminateSpreadsheetReportBuilder.FailureModeType.BOTH
Both failure index type
|
static LaminateSpreadsheetReportBuilder.FailureModeType |
LaminateSpreadsheetReportBuilder.FailureModeType.IN_PLANE_PLY
Ply failure index
|
static LaminateSpreadsheetReportBuilder.FailureModeType |
LaminateSpreadsheetReportBuilder.FailureModeType.INTERLAMINAR
Bonding failure index
|
Modifier and Type | Method and Description |
---|---|
LaminateSpreadsheetReportBuilder.FailureModeType |
LaminateSpreadsheetReportBuilder.failureMode()
Returns the failure mode
License requirements: None. |
static LaminateSpreadsheetReportBuilder.FailureModeType |
LaminateSpreadsheetReportBuilder.FailureModeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LaminateSpreadsheetReportBuilder.FailureModeType |
LaminateSpreadsheetReportBuilder.FailureModeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LaminateSpreadsheetReportBuilder.FailureModeType[] |
LaminateSpreadsheetReportBuilder.FailureModeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LaminateSpreadsheetReportBuilder.setFailureMode(LaminateSpreadsheetReportBuilder.FailureModeType failureMode)
License requirements: nx_lam_composites ("Laminate Composites") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.